Can LPS22HB be used to measure liquid pressure inside miniature container with NACL solution
Can LPS22HB be used to measure liquid pressure inside a miniature container with NACL solution. The sensor will be mounted at one end of the tube like container (4mm diameter). The pressure inside the liquid will keep changing due to the pressure applied from the other side of the tube. Do you think this sensor can be used in such environment ? The pressure range would be within the specified range if this sensor.
Also how do you compare LPS22HB with LPS28DFW ?
thanks