Can we "deGauss" the LIS2MDL using register commands to reset the AMR when exposed to high field to remove large hard iron offsets? The MMC5983MA allows this, does the LIS2MDL?
We have noticed that several LIS2MDL have come back to us with very large magnetic field offsets. While these can be corrected by the usual offset calibration, the large offsets are due to exposure to a large magnetic field source somewhere in the environment. We would like to be able to remagnetize the anisotropic MR film to recover its factory magnetization. Is this possible using the embedded current drivers for the offset cancellation in the LIS2MDL? The MMC5983MA offers this feature. We would like to use it for the LIS2MDL if available.