Skip to main content
Visitor II
October 1, 2021
Question

Can we use Hall Sensor as main sensor and no auxiliary sensor to run the motor? Can we control the speed of the motor? how to decide the placement electrical angle? Default 300 in Workbench.

  • October 1, 2021
  • 11 replies
  • 3695 views

Hi, I am using Motor Control workbench to run the motor using Nucleo-F446RE and X-NUCLEO-IHM08M1. Initially I used Main Sensor "Observer+PLL" and auxiliary sensor "Hall Sensor" and I can able to control the motor. Now our requirement is to use only hall sensor as Main sensor. In this case the motor is able to run but at a fixed speed and not varying to any change in parameters.

Thank you.

Regards

Vijay Ganisetti.

    This topic has been closed for replies.

    11 replies

    VGani.1Author
    Visitor II
    October 7, 2021

    Hi @cedric H​ ,

    Thank you for your responses. Yeah I just want to make sure that whether my idea of placement of electrical angle is correct.

    Regards

    Vijay