Cannot get data from the SensorTile.Box into the Watson IoT Platform
I am using Algobuilder to setup a dumb application to get the acceleration from the SensorTile.Box. I compile it using the BLE template and connect the box ST BLE Sensor Android App. The connection between the App and the Watson IoT Platform is correct and I see my device in the Platform dashboard but I do not get any data. Moreover, I hit start logging in the mobile phone App but no csv file is created. I even tried to use Unicleo GUI with BLE capability enabled but I cannot see anything because the PC Bluetooth configuration cannot connect to the Box.
If I compile the dumb application without the BLE template, everything works: I can get the data with Algobuilder and Unicleo GUI through the COM port.
What is wrong??
Last week I could connect to the Watson IoT Platform and get the data correctly and now, it does not work?
Any idea?
Regards