Configure interrupt for LIS2DH12
I am trying to configure an interrupt on a LIS2DH12 in order to detect when the device is being hit.
I tried just configuring one axes to generate the interrupt. But Interrupt is never being fired (Or it is fired constantly). This is my current configuration:
20---- 67
21---- 0 22---- 40 23---- 0 24---- 8 25---- 0 26---- 0 27---- ff 28---- 40 29---- 0 2a---- c0 2b---- ff 2c---- 80 2d---- 44 2e---- 0 2f---- 20 30---- 10 31---- 55 32---- 40 33---- 0 34---- 0 35---- 0 36---- 0 37---- 0 38---- 0 39---- 0 3a---- 0 3b---- 0 3c---- 0 3d---- 0 3e---- 0Leaving the device over the table where I work, gives a constant measurement of:
x: 0 y: 0 z: 63
And int1Source register gives 0x25 which seems to be 0010 0101. I have just configured ZLow to trigger the interrupt but I get that XL, YL and ZH but not IA so interrupt is not generated by register. INT1 pin is always on in this case.
What should I do in order to configure a movement in any of the 3 axis? I want that my device stays in a position and detect any movement in any of the axes configured over the threshold set(For example, any movement higher than 1G). But I think I cannot detect at the same time ZH or ZL, XL or XH or YL or YH. I mean, if the device reads 64, trigger an interrupt over 0 or 128 in that axes. Is this possible?
#lis2dh12