Connecting iNEMO v2 Board UART to Bluetooth
Dear all,
I have STEVAL-MKI062V2, I could be able to compile code using IAR EW. There is COM connector for the board ( UART2 pins of STM32), jumper J4. ST says,Note: J4 does not offer any transceiver; it is directly connected to the microcontroller pins. As this prevents any overload/over-voltage on these pins.Moreover, J4 connector also provides a 3.3 V pin which can be used to supply a RS232 transceiver. Sinking too much current from this pin could damage the board.
I want to connect J4 of iNEMO to the UART bluetooth module for wireless connection to PC.I have Bluetooth Mate Gold fromhttp://www.sparkfun.com/products/9358
which has the following electrical connection for Arduino based AHRS modulehttp://www.sparkfun.com/products/10736
I sketched electrical connections to J4 of iNEMO below. I'm not sure to go with this because I'm afraid iNEMO may be damaged.