Custom algorithms using finite state machine (FSM) on LSM6DSO sensor.
Hello, there,
I would like to know about the application of FSM feature of LSM6DSO sensor.
I can see in the example that every embedded functions are implemented using FSM.
We have developed three algorithm and looking at implementing via state machine diagram.
Can FSM be used for our custom algorithms?
Does FSM only supports sensor's internal features such as 4D, Free Fall, Wrist-tilt, Basic Pedometer, Motion and so on?
Kind regards,
Aakash Soni.