Data Acquisition Problem
Hi ,
i am trying to capture accelerometer data from LIS3DSH triaxial sensor using NORDIC nrf5232 Soc., via i2c for a configuration of 1600 samples/sec. as it supports two slave address 1D & 1E .
when i configure for 1d and capture data is not coming properly like 0 data or some constant data , but if i configure the same for 1e data is properly coming , only problem being 0 at some sample set. nrf52832 is set for 400 k clock , when seen in logic analyzer while capturing i am getting 200K and also in oscilloscope, i have asked the issue with Nordic as well , they say code wise everything is fine with respect to code , also without connecting to slave clock generated is also 400K.
so help me with this issue , how to overcome.
Thank you