Deformation measurment of metall reactor
Dear all,
I am interested in the MEMS accelerometer (IIS3DWB) to measure radial and maybe vertical movement of a metall reactor. The maximum g range of the movement should be 4-5 g. And the vibration frequency should be 0.5-2 kHz. I would install approximately 6-8 sensors at orthogonal positions on the reactor (3-4 meters apart).
Now I would like to ask you, if you could suggest a combination of components with which the accelerometer can be used. The goal would be to install the sensor combined with an evaluation board, or whatever you suggest, directly on the reactor. We would then need a way to transfer the raw data on a computer system. The data sampling frequency should be as high as possible (around 10kHz).
Thank you in advance for your help!