Question
Details on filtering of Accelerometer
Trying to understand the internal mechanics of the accelerometer I'm using a bit better.
Specifically, I'm using a H3LIS331DL.
I have settings that will look like this:
ODR = 1,000 Hz
BW = 500 Hz
Filter = 780 Hz
However, there's not much detail in the datasheet on the filtering. Is that the 3dB point?
If there was a 100g 1,000 Hz impulse - would I be expecting 0g as a reading?