Diference between LSP27HHW and LSP27HHWT?
The LSP27HHW also embeds a temperature sensor.
Comparing the datasheet, I can´t find any diference.
Why LPS27HHTW is 1€ more expensive?
The LSP27HHW also embeds a temperature sensor.
Comparing the datasheet, I can´t find any diference.
Why LPS27HHTW is 1€ more expensive?
Hi @APere.7 ,
the difference between the two part numbers relies on the fact that the LPS27HHTW not only has an embedded temperature sensor, but is also calibrated at production level to guarantee a Temperature accuracy in the ±1.5 °C range, as you can see from the datasheet, p.1.
This is the price difference root cause: however, if you have a temperature reference on your system, you can of course calibrate the LPS27HHW embedded temperature sensor (in offset at 25°C and gain versus temperature in the defined range) via software, getting the desired accuracy. This is useful especially in post-solder condition.
-Eleon
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.