Skip to main content
Visitor II
July 24, 2020
Question

ERROR MESSAGE

  • July 24, 2020
  • 1 reply
  • 558 views

HI everyone,

I have this error message when I compile my main program with eclipse ... I'm using a P Nucleo 53L0A1 .. someone can tell me what's happening because I really don't understand

error message =>

Open On-Chip Debugger 0.10.0+dev-00021-g524e8c8 (2019-04-12-08:48)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

C:/Ac6/SystemWorkbench/plugins/fr.ac6.mcu.debug_2.5.0.201904120827/resources/openocd/scripts/st_board/nucleo_l476rg.cfg:15: Error: Can't find target/stm32l4.cfg

in procedure 'script' 

at file "embedded:startup.tcl", line 60

at file "C:/Ac6/SystemWorkbench/plugins/fr.ac6.mcu.debug_2.5.0.201904120827/resources/openocd/scripts/st_board/nucleo_l476rg.cfg", line 15

    This topic has been closed for replies.

    1 reply

    ST Employee
    July 24, 2020

    ​Hello,

    I would use the example code provided in X-CUBE-53L0A1 to check if your AC6 IDE is working and base on the example code structure to develop your own code.

    Thanks,

    Julien