Error while inserting the STM Linux driver
hello,
I am trying to get the LSMDSO32 to work with https://github.com/STMicroelectronics/STMems_Linux_IIO_drivers branch 4.19 built on 5.4 kernel.
I am able to build the kernel image on 5.4
But when i try to insmod the modules i get the following errors.
Any one came across this or know what is the issue?
# insmod st_lsm6dso32.ko
[ 3073.698696] st_lsm6dso32: Unknown symbol devm_iio_kfifo_allocate (err -2)
[ 3073.706025] st_lsm6dso32: Unknown symbol devm_iio_triggered_buffer_setup (err -2)
insmod: failed to load st_lsm6dso32.ko: No such file or directory
# insmod st_lsm6dso32_i2c.ko
[ 3079.860966] st_lsm6dso32_i2c: Unknown symbol st_lsm6dso32_probe (err -2)
[ 3079.868030] st_lsm6dso32_i2c: Unknown symbol st_lsm6dso32_pm_ops (err -2)
insmod: failed to load st_lsm6dso32_i2c.ko: No such file or directory
#
device tree:
lsm6dso32@6a {
compatible = "st,lsm6dso32";
reg = <0x6a>;
};