Skip to main content
Visitor II
October 3, 2018
Question

Example acceleration data - LIS3DH

  • October 3, 2018
  • 2 replies
  • 831 views

Section 4.2.3 of the application note for the LIS3DH sensor provides example register values for various sensor readings. For +/-2g at high resolution mode the typical sensitivity is 1mg/unit. When BLE=0, I see why registers 28h and 29h are E0h and 15h respectively (for a 350mg reading). However, I do not see how a 1g = 1000mg reading is 00h and 40h in those two registers. Would this not be for a sensor reading of 1024mg instead? ​I would think the sensor reading should be 80h and 3Eh to provide correct 1g result.

    This topic has been closed for replies.

    2 replies

    MGAuthor
    Visitor II
    October 3, 2018

    Also, I realize that at 12-bit resolution the output range is -2048 to +2047 and that mapping -2g to +2g to this range would have 1g mapping to 1024, but 350mg would not map to 350.​

    ST Employee
    October 4, 2018