FlightSense part with fastest sample rate
My application is uses a linear array (18 sensors) for object presence detection at a fixed distance (~70mm). A range threshold setting is used. The range measurement is not read, only the interrupt is used indicating the presence of a moving object. The preferred minimum sample rate would be around 60 Hz, but faster would be better. The sensors are always used indoors but the item to be sensed is black with a relatively reflective surface. I have a working prototype using the VL6180X but looking for a faster sensor.
Which part provides the fastest sample rate for this application?