Skip to main content
Visitor II
December 27, 2022
Question

For X-NUCLEO-IKSO1A3 and NUCLEO-L476RG only options IKSO1A1 and IKSO1A2 which are working well but not option IKSO1A3 with STM32CubeExpansion_MEMS1_V4.4.1

  • December 27, 2022
  • 1 reply
  • 736 views

in order to get all sensor working

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    January 10, 2023

    Hello @PWeil.2​,

    You are right, the X-CUBE-MEMS1 expansion package version 4.4.1 supported the STM32L476RG devices and NUCLEO-L476RG board with X-NUCLEO-IKS01A1 and X-NUCLEO-IKS01A2 Boards.

    You can check this history and main changes in the "Release notes" file of the package.

    Note that the NUCLEO-L476RG examples and applications are replaced by NUCLEO-U575ZI-Q ones, since the release V9.3.0 of X-CUBE-MEMS1 expansion package.

    When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

    Imen