FSM_START_ADDRESS in LIS2DUX12
Hello,
The LIS2DUX12 datasheet clearly states that "12.1.3 FSM_START_ADD_L (58h) and FSM_START_ADD_H (59h) FSM start address register (R/W). First available address is 0x35C.".
The default address in MEMS-studio is 0x0200. In the FSM examples on GitHub, the address also is the same: 0x0200.
Why are these addresses different and which one is correct?