Skip to main content
Visitor II
May 6, 2024
Solved

Getting started with STEVAL-MIC007V1

  • May 6, 2024
  • 1 reply
  • 852 views

Hi Everybody,

 

I am a beginner and I need some information to start using the following devices:

- Nucleo-F401RE

- X-Nucleo-Amicam1

- Steval-mic007v1.

 

I have currently downloaded the following material:

- X-cube-memsmic1

- Link007

- Link009

- Stm32cubeid.

Is it necessary to install additional software tools and/or embedded software?

 

Is it possible to get an initialization procedure or a video guide for the correct configuration of the devices for the use of the Steval-mic007v1 microphones?

 

Thanks for your help.

 

Best wishes,

 

Oscar

 

    This topic has been closed for replies.
    Best answer by SimonePradolini

    Hello @OsBo 

    X-NUCLEO-AMICAM1 + STEVAL-MIC007V1 is natively supported in X-CUBE-MEMSMIC1 in conjunction with NUCLEO-L476RG and NUCLEO-L4R5ZI only. 

    By using the above-mentioned setup, you can go through the AMICAM1/Microphone_Streaming examples available in X-CUBE-MEMSMIC1. All the details are available in the User Manual.

     

    Best regards

    Simone

    1 reply

    Technical Moderator
    May 23, 2024

    Hello @OsBo 

    X-NUCLEO-AMICAM1 + STEVAL-MIC007V1 is natively supported in X-CUBE-MEMSMIC1 in conjunction with NUCLEO-L476RG and NUCLEO-L4R5ZI only. 

    By using the above-mentioned setup, you can go through the AMICAM1/Microphone_Streaming examples available in X-CUBE-MEMSMIC1. All the details are available in the User Manual.

     

    Best regards

    Simone