Getting wrong register value when reading "WHO_AM_I" register on I3G2450D mems. (STM32F429ZIT)
I'm using the following driver: STMems_Standard_C_drivers/i3g4250d_STdC at master · STMicroelectronics/STMems_Standard_C_drivers (github.com)
You can ignore the details of the driver code but the important thing to note is that
The driver requires you to write your own "platform_read" function since this is platform dependent.
I am using SPI and this is how my implementation looks like:
static int32_t platform_read(void *handle, uint8_t reg, uint8_t *bufp, uint16_t len)
{
uint32_t msTimeOut = 1000;
reg |= 0x80;
//I3G2450D_CS_ENABLE;
HAL_GPIO_WritePin(MEMS_CS_GPIO_Port, MEMS_CS_Pin, GPIO_PIN_RESET);
HAL_SPI_Transmit(handle, ®, 1, msTimeOut);
HAL_SPI_Receive(handle, bufp, len, msTimeOut);
//I3G2450D_CS_DISABLE;
HAL_GPIO_WritePin(MEMS_CS_GPIO_Port, MEMS_CS_Pin, GPIO_PIN_SET);
return 0;
}When using this function to read the "WHO_AM_I" register (Address: 0x0FU) I am supposed to get the hex value "0xD3U" (Decimal: 211) but the function call sets the wrong value in "bufp". I get hex "0xd4", following is a screenshot from a debugging session:
"whoamI" is the value that gets sets from reading the register and "I3G240D_ID" is the expected value.
In binary the expected value is: 11010011, this is correct according to manual of the gyroscope, but what I get is: 11010100.
My SPI init:
static void MX_SPI5_Init(void)
{
/* USER CODE BEGIN SPI5_Init 0 */
/* USER CODE END SPI5_Init 0 */
/* USER CODE BEGIN SPI5_Init 1 */
/* USER CODE END SPI5_Init 1 */
/* SPI5 parameter configuration*/
hspi5.Instance = SPI5;
hspi5.Init.Mode = SPI_MODE_MASTER;
hspi5.Init.Direction = SPI_DIRECTION_2LINES;
hspi5.Init.DataSize = SPI_DATASIZE_8BIT;
hspi5.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi5.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi5.Init.NSS = SPI_NSS_SOFT;
hspi5.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;
hspi5.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi5.Init.TIMode = SPI_TIMODE_DISABLE;
hspi5.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi5.Init.CRCPolynomial = 10;
if (HAL_SPI_Init(&hspi5) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI5_Init 2 */
/* USER CODE END SPI5_Init 2 */
}What I have tried (without success):
- Changing the baud rate prescaler.
- Changing first bit from MSB to LSB. (manual says data is sent MSB first but I thought trying was worth it.)
- changing CPOL to "High"
- changing CPHA to "2 Edges" (note when I change this in combination with CPOL I get different results (decimal 255) but still not the correct one)
- double checked Chip Select line (according to manual PC1 is the correct CS line for the I3G2450D)
- set a delay after setting CS line to high/low
- set a delay before/after reading with SPI_Transmit / SPI_Recieve
I'm out of options as to what the problem could be (other than hardware related), google suggests trying the same things I did above so maybe someone with more experience knows a solution.
Regards,
Fatih