Question
H3LIDS331DL: Impossible to get INT1 with THRESHOLD and DURATION working !
Hello,
I can succesfully have ready (DRDY) under interrupt (INT1) at low or normal power vfrequencies. Cool.
BUT I do not success in using threshold and duration.
Can anyone, can give me the correct configuration to do this:
- Get an INT1 interrupt each time the sensor as over pass a threshold for more than 50 samples at 10Hz low power.
- And then do necessary process in the interrupt to renew this indefinitly.
- The threshold can be 0 for now to ensure that the sensor will create an interrupt periodically each 5 s
In advance many thanks