H3LIS - low power optimize impact or impulse detect
I want to optimize the low power mode of my H3LIS331DL to detect an impact. I've attached an image of a scope capture of the current draw of my board during sleep mode. I've determined that the large current draw pules are the accelerometer turning on. The low power frequency in the capture (10Hz) gives me the most responsive detection. However, that pulse is huge! 40ms wide and 300uA is way too much for this application. What's the best way to optimize the power in this case? What strategies can I use? Is 300uA really the baseline current draw when the accel turns on? Or am I missing a setup parameter that can lower that baseline draw?