H3LIS100DL sleep-to-wake - how to enable?
Greetings. I am familiar with the general sleep-to-wake functionality, I've used it successfully in the IIS2DH. However I am having issues with the H3LIS100DL. I believe I've enabled sleep-to-wake using control register 5, I've configured the interrupt using int1_cfg, int1_duration and int1_ths, and I can view interrupt events occurring using the Unico interface. However I cannot "see" the change in output data rate from an interrupt state to a non-interrupt state in the Unico plot screen. Admittedly not scientific, however the transition was very obvious when using the IIS2DH.
Based on my understanding, when the interrupt is active, I should have a ODR per the setting in ctrl_reg1 (400Hz in my case) and the power mode should jump from low power to normal mode. While not explicitly stated, my assumption is that, in the low power/interrupt-not-active state, the ODR should be 10Hz max (since this is the max possible in low power mode). If this is true, then certainly I should be able to see (via Unico) the ODR change from 10Hz to 400Hz.
I did also notice that control register 5 auto updated after an interrupt event. To enable sleep-to-wake mode, control register 5 is set to 0x03. After an interrupt, it auto updates to 0x01. Not sure why, not sure of the implications, just merely an observation (perhaps it is indicative of something I am doing wrong).
Anyway, any assistance to getting this set up properly would be very helpful. Like I said, I have the host board and the Unico interface, so I can tweak/test quickly.
Thanks,
Chris