H3LIS200DL interrupt threshold meaning
Hi, all.
I am trying to figure out H3LIS200DL interrupt issue. Even if I have set interrupt threshold to high value, I can't see any pulse on INTx line. Also not sure what the INT1_THS register describes. Datasheet shows only 7 bit value.
What I have done is as following.
/* initialized */
...
if (h3lis200dl_device_id_get(h3lis200dl->ctx, &whoamI) != HAL_OK) {
sprintf(pBuf, "Failed to get chip id\r\n");
tx_com((uint8_t*)pBuf, strlen(pBuf));
}
sprintf(pBuf, "Chip ID: %x \r\n", whoamI);
tx_com((uint8_t*)pBuf, strlen(pBuf));
if (whoamI != H3LIS200DL_ID) {
sprintf(pBuf, "Couldn't get valid chip id\r\n");
tx_com((uint8_t*)pBuf, strlen(pBuf));
while (1) {
/* manage here device not found */
}
}
/* Configure filtering chain */
/* Accelerometer - High Pass / Slope path */
h3lis200dl_hp_path_set(h3lis200dl->ctx, H3LIS200DL_HP_DISABLE);
h3lis200dl_pin_polarity_set(h3lis200dl->ctx, H3LIS200DL_ACTIVE_HIGH);
/* Set minimum event duration for free fall */
h3lis200dl_int1_dur_set(h3lis200dl->ctx, 3);
/* Apply free-fall axis threshold
* Set threshold to (350mg -> 22)
*/
h3lis200dl_int1_threshold_set(h3lis200dl->ctx, 127);
/* Enable interrupt generation on free fall INT1 pin */
h3lis200dl_int1_on_threshold_mode_set(h3lis200dl->ctx,
H3LIS200DL_INT1_ON_THRESHOLD_OR);
h3lis200dl_int1_on_threshold_conf_get(h3lis200dl->ctx, &int_route);
int_route.int1_xlie = PROPERTY_ENABLE;
int_route.int1_ylie = PROPERTY_ENABLE;
int_route.int1_zlie = PROPERTY_ENABLE;
h3lis200dl_int1_on_threshold_conf_set(h3lis200dl->ctx, int_route);
// h3lis200dl_int1_notification_set(h3lis200dl->ctx, H3LIS200DL_INT1_LATCHED);
/* Set Output Data Rate */
h3lis200dl_data_rate_set(h3lis200dl->ctx, H3LIS200DL_ODR_50Hz);
...
/* reading operation to clear interrupt bit in INT1_SRC */If AOI of INT1_CFG is OR, INT1 line is always active. Can you explain the INT1_THS meaning in detail?
Thanks in advance.
honestech