H3LIS200DL Readings and Conversion
Hello:
I am getting some bizarre values from this device, and maybe it's not configured correctly, or I am not reading it correctly.
It appears I can send and read from the device. I can use the 'WHO_AM_I' and get back the value 32, which is correct. I then set the control register 1 at 0x20 to 0x27 = b00100111, which sets PM to normal, and x, y and z enabled. To check if the register has taken the value, I read it back, and it says 0x27.
I'm assuming then that after doing this, I can just read the output registers at x,y and z, and I am doing reads every 100ms (I do not have the interrupts configured at this point, and for now, not converting from two's complement)
However, I am unable to get the output registers to change from 0xFF, no matter what I do with the board it's mounted on. I have tried some pretty hard 'nudges' and it will not change. Additionally, if I continuously read the status register, it is always 0xEE, which makes little sense.
Can someone provide some insight as to what might be going wrong?
Thanks for your help!
Roger.