H3LIS331DL configuartion issues
Hi,
I am working with H3LIS331DL sensor . my configuration is as follows
- 1Power on the sensor
- configure the control register 1 with normal power mode and data rate 1000hz
- configure interrupt source1 for data ready interrupt
- GPIO call back registered for data ready interrupt.
This scenario is working fine. we are sampling after getting the data ready interrupt.
I have some special cases where i am facing some issues.
if there is some delay in step 2 and step 3 due to some other register configuration example configuring thecontrol register 4 then (in between step 2 and 3)i am not getting the data ready interrupt. This is one issue.
Next one is after step 4 if get data ready interrupt in case if i delayed to clear the data ready interrupt by reading the data for more than 3 msec then next data ready interrupt is not triggering.
could you help me is there is sequence needs to be followed?
or what could be the reason for the above 2 issues.
thanks in advance.
with Regards,
Thangaraj.P
Note: this post was migrated and contained many threaded conversations, some content may be missing.