Skip to main content
Visitor II
September 28, 2015
Question

Hardfault error while running osxMotionAR example project

  • September 28, 2015
  • 0 replies
  • 528 views
Posted on September 28, 2015 at 13:17

I am getting one hardfault error after calling the osx_MotionAR_Initialize() API. I am using STM32F401 Nucleo board with X-NUCLEO-IKS01A1 sensor expansion board. I have installed required software and i tried to run the example project available from the directory Projects\STM32F4xx-Nucleo\Applications\DataLogActivity\EWARM in IAR IDE. But i am getting hardfault after calling osx_MotionAR_Initialize() API.What could be the problem? i didn't changed anything in the project, just opened the existing project in the workspace. I have tried the same in keil also but result is same. Please help me to figure out the problem.

As per the user guide i have edited the osx_license.h file. I am getting license error when osx_mar_license[3][4]  buffer filled with zeros. After editing the license buffer with license, i am getting hardfault error.

License wizard generate following three codes

Node Code: 1932DD005128B2C33690DA1103A823AA

Site Code: ADBE59CA8D03254E20F816DD334B46E8

License Code: 5D1E454C6584BFE888D1AC4F787B0850

and i edited buffer as shown below. Is there any mistake in this?

//uint32_t osx_mar_license[3][4] =

//{

// { 0x1932DD00, 0x5128B2C3, 0x3690DA11, 0x03A823AA },

// { 0xADBE59CA, 0x8D03254E, 0x20F816DD, 0x334B46E8 },

// { 0x5D1E454C, 0x6584BFE8, 0x88D1AC4F, 0x787B0850 }   

//}; 

    This topic has been closed for replies.