Question
Hello, Can you please suggest STM MCU/MPU part which is used for 3 phase metering applications?
We are looking for the MCU parts which should have below features.
- 512Kb flash, 64Kb RAM
- 12 Bit 12-16 channels Delta Sigma ADCs
- SPI,I2C, UART, CAN, USB2.0
- LCD Interface
- External RAM interface up to 512Mb
- External Flash interface up to 64Mb
- 80 -100 GPIOs
- DAC
- SD/MMC Interface
Thanks,
Brijesh K.