Skip to main content
Visitor II
September 10, 2020
Solved

Hello Sir, We used LSM6DSMTR this part in our medical device application. 1. LSM6DSMTSensor Part is FDA approved 2. EoL of 6 axis

  • September 10, 2020
  • 1 reply
  • 596 views

We used LSM6DSMTR this part in our medical device application.

1. LSM6DSMTSensor Part is FDA approved

2. EoL of 6 axis

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi @Vmist.1​ ,

    please note first that none of the ST iMUs is qualified for medical standards. The usual flow is that the customer qualifies his medical application with the proper procedure: if the application as a whole passes the qualification steps, the entire device and its components can be declared medical level.

    Coming to your questions:

    >> 1. LSM6DSMTR Sensor Part is FDA approved

    No, the sensor is not part of Food & Drugs administration policy.

    >> 2. EoL of 6 axis

    The lifetime of a standard ST sensor is less then 10 years, typically 5 or 6 years. However, ST portfolio offers also sensors with a 10-year longevity commitment. The suggested sensor satisfying this criterion is the ISM330DHCX, tailored for Industry 4.0 applications. If it is possible for you, with respect to the maturity of your application, I would suggest you to use this sensor.

    -Eleon

    1 reply

    ST Employee
    September 11, 2020

    Hi @Vmist.1​ ,

    please note first that none of the ST iMUs is qualified for medical standards. The usual flow is that the customer qualifies his medical application with the proper procedure: if the application as a whole passes the qualification steps, the entire device and its components can be declared medical level.

    Coming to your questions:

    >> 1. LSM6DSMTR Sensor Part is FDA approved

    No, the sensor is not part of Food & Drugs administration policy.

    >> 2. EoL of 6 axis

    The lifetime of a standard ST sensor is less then 10 years, typically 5 or 6 years. However, ST portfolio offers also sensors with a 10-year longevity commitment. The suggested sensor satisfying this criterion is the ISM330DHCX, tailored for Industry 4.0 applications. If it is possible for you, with respect to the maturity of your application, I would suggest you to use this sensor.

    -Eleon