Question
Hello, We are carrying out experiments using lis3dsh accelerometer. With ODR set to say, 50Hz and INT1 enabled, we are seeing the INT1 coming at ~48Hz instead of 50Hz We are unable to find any document on internal clock spec It would help if we could
Posted on May 28, 2018 at 16:17
Please find the register settings as below
NameAddressValue
CTRL_REG3
0x23
0XE8
CTRL_REG4,
0x20
0X67
CTRL_REG5
0x24
0XC0
CTRL_REG6
0x25
0X10
FIFO_CTRL
0x2E
0X0