Question
Hello, Why can I not use 'Program with bootLoader' for FOTA in function packs like 'en.fp-sns-allmems1_firmware_v4.1.0', and 'en.fp-sns-allmems2_v2.1.0' that provide two different binaries?
Hardware: SensorTile.box
The project readme.txt file suggests that the software should start from the memory address 0x08004000 in FLASH.
- How can I change this when I am downloading the software from the Android app?
- The board has to be restarted after the software is downloaded on the sensor, can I eliminate this restart process in any way?
Regards
Aditi Prakash