Skip to main content
Visitor II
May 13, 2019
Question

Help with programming the STM32 STEVAL-STLCS01V1 (with the STEVAL-STLKT01V1 Sensor development kit) using Arduino Uno sketch IDE.

  • May 13, 2019
  • 0 replies
  • 599 views

I want to program the mcu STM32 STEVAL-STLCS01V1. I have the STEVAL-STLKT01V1 Sensor development kit and i've read that i can mount the STLCX01V1 on the Arduino Uno board, mount the STEVAL-STLCS01V1 on the STLCX01V1 board. and then use the Arduino sketch IDE to program the STEVAL-STLCS01V1 micro-controller.

I have some follow-up questions:

1. Am i correct? can i do that (program the STEVAL-STLCS01V1 using the Arduino Uno and the Arduino IDE, when i connect the board as i explained above)?

2. If i can program the STEVAL-STLCS01V1 using the Arduino Uno IDE, do i need to add some libraries to my sketch? or do something else before i write my code (like i write any other code for Arduino)?

3. Do you have more instruction that i need to know when i program the micro-controller with the Arduino IDE?

Thank you very much for your help,

Reshef Finkelstein

    This topic has been closed for replies.