High Frequency Noise From STWINMA2A
Hello everyone,
I am currently working with STWIN+STWINMA2A microphone array for ultrasonic signal processing. I use the firmware "AMicArray_Microphones_Streaming" and connect the board directly to my laptop as an USB microphone.
However, the data suffers from significant noise with certain frequencies.
I used Audacity to sample the data in an quiet environment, with the configuration as figure 1. The sampling rate is 96kHz.

The DFT of 10,000 data points is shown in the next figure, we can see a very high noise level at around 40k, 24k, and 8kHz.

Is there any thing I can do to fix this problem?
Thanks!