High Pass filter on LSM6DS3?
Hi,
We are running a vibration analysis system based on the LSM6DS3. This is FIFO based, and everything works as expected. Application is accel only.
However when enabling the high pass filter from the digital composite filter, all readings out of the FIFO are 0. Data is still provided at expected intervals. Clearly the data has values ABOVE filter.
Should enabling the filtering not be as simple as writing the correct value to register CTRL8_XL?
something like (0x17, 0b00100100). We tried configuring before starting accel (0x10) and / or fifo (0x0A). Same result.
Many thanks for any input.
br
Christophe