Question
Housing for inclinometer using MEMS, that leads to low deviation over a temperature range from -10°C to 40°C?
(1) Are there best practice examples available?
(2) Can I glue the top side of the MEMS to a steel surface? I expect lower temperature deformation than when fixed with the PCB. Or does the steel surface deform the MEMS in the mentioned temperature rage and thus lead to bad measurements?
(3) Which glue would you suggest?