How to apply Pedometer Regression output (.ucf/.json) for SensorTile.box Pro?
Hi ST Community,
I am working on a project using the SensorTile.box Pro. My goal is to implement a highly accurate step counter using the LSM6DSV16X's embedded pedometer.
What I have done:
I recorded data patterns at 30Hz and successfully ran the Pedometer Regression Tool in MEMS Studio.
The tool generated the optimum configuration files (pedometer.json ).
I converted these register settings into a .ucf file format.
The Problem: I need to apply these "Golden Settings" to the sensor initialization in AlgoBuilder so they persist after a reset. However, I am unable to find a standard method to load this configuration:
I checked the Sensor Hub block properties, but I do not see a "Load Configuration/UCF" option.
I searched the Library for a "Register Write" block to manually input the values, but this block seems missing or hidden in my version of AlgoBuilder (I only see Acceleration, FSM/MLC, Sensor Hub, etc. under the Sensor Hub folder).
My Question: What is the correct way to inject a custom register configuration (or load a .ucf file) for the LSM6DSV16X sensor in the SensorTile box Pro?
Is there a specific block I should use (e.g., the FSM/MLC block as a container)?
Or do I need to use a Custom Code block? If so, what is the syntax for writing registers during initialization ?
Hardware/Software Details:
Board: SensorTile.box Pro (STEVAL-MKBOXPRO)
Sensor: LSM6DSV16X
Software: AlgoBuilder (v2.2.0), MEMS Studio
Any guidance or a screenshot of the correct block setup would be greatly appreciated!
Thanks.