Skip to main content
Visitor II
June 9, 2025
Question

How to Change Sampling Frequency for ST BLE Sensor App

  • June 9, 2025
  • 1 reply
  • 453 views

Hello STM32 Community,

I’m currently working with the STEVAL-PROTEUS1 evaluation board, which integrates an STM32WB5MMG microcontroller and an IIS2DLPC MEMS accelerometer. I’m using the board together with the ST BLE Sensor mobile app, and it works great out-of-the-box for streaming sensor data over BLE.

However, I’d like to change the sampling frequency (ODR) of the onboard accelerometer to suit my specific application needs. For example, I want to increase the data rate to 800 Hz, instead of the default (which seems to be 25 Hz or 50 Hz).

What I’ve done So Far:

 

int32_t IIS2DLPC_Init(IIS2DLPC_Object_t *pObj)

{

  /* Enable register address automatically incremented during a multiple byte

  access with a serial interface. */

  if (iis2dlpc_auto_increment_set(&(pObj->Ctx), PROPERTY_ENABLE) != IIS2DLPC_OK)

  {

    return IIS2DLPC_ERROR;

  }

  /* Enable BDU */

  if (iis2dlpc_block_data_update_set(&(pObj->Ctx), PROPERTY_ENABLE) != IIS2DLPC_OK)

  {

    return IIS2DLPC_ERROR;

  }

  /* FIFO mode selection */

  if (iis2dlpc_fifo_mode_set(&(pObj->Ctx), IIS2DLPC_BYPASS_MODE) != IIS2DLPC_OK)

  {

    return IIS2DLPC_ERROR;

  }

  /* Power mode selection */

  if (iis2dlpc_power_mode_set(&(pObj->Ctx), IIS2DLPC_HIGH_PERFORMANCE) != IIS2DLPC_OK)

  {

    return IIS2DLPC_ERROR;

  }

  /* Select default output data rate. */

  pObj->acc_odr = 800.0f;

  /* Select default operating mode. */

  pObj->acc_operating_mode = IIS2DLPC_HIGH_PERFORMANCE_MODE;

  /* Select default low noise (disabled). */

  pObj->acc_low_noise = IIS2DLPC_LOW_NOISE_DISABLE;

 

  /* Output data rate selection - power down. */

  if (iis2dlpc_data_rate_set(&(pObj->Ctx), IIS2DLPC_XL_ODR_800Hz) != IIS2DLPC_OK)

  {

    return IIS2DLPC_ERROR;

  }

  /* Full scale selection. */

  if (iis2dlpc_full_scale_set(&(pObj->Ctx), IIS2DLPC_2g) != IIS2DLPC_OK)

  {

    return IIS2DLPC_ERROR;

  }

  pObj->is_initialized = 1;

  return IIS2DLPC_OK;

}

 

I’m Trying to Achieve:

  • Stream real-time accelerometer data at 800 Hz over BLE to a mobile device using the ST BLE Sensor app.

  • Maintain stable BLE communication without data loss or overflow.

Any guidance, example code snippets, or references to documentation would be greatly appreciated. I believe others working with STEVAL-PROTEUS1 and similar BLE sensor nodes might benefit from this as well.

Thanks in advance!

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    June 12, 2025

    Hi @Tunahan ,

    The official firmware also supports ODR of 800Hz, have you tried changing the ODR via app instead of modifying the code?