How to configure and read data from Sensortile box through python script
I just started working with the Sensotile box (STEVAL-MKSBOX1V1). I managed to upload the datalogger binary to the module (from the FP-SNS-STBOX1 function pack) and configured the sensors to acquire data via Unicleo GUI.
Now I want to use a python script for the configuration of the sensors via USB cable instead of using Unicleo GUI.
1 - Can someone share if it's possible to acquire accelerometer data from the module in high-performance mode with high sensitivity?
2- Is it possible to acquire data at high performance over bluetooth?
3- Is there any existing function pack that supports the functionality with python-like FP-SNS-DATALOG1 does it for STWIN?
Any information on this will be very helpful. Thanks