Skip to main content
Visitor II
June 11, 2018
Question

How to connect HTS221TR via 3-wire SPI to uC? Is there any schematics or application note?

  • June 11, 2018
  • 1 reply
  • 467 views
Posted on June 11, 2018 at 11:35

HTS221TR connecting via 3-wire SPI.

Is there any official app. note for this interface.

I suppose it is via connection MOSI and MISO through 10K resistor and then feeding it to a sensor.

But I would like to get some official input from STM because I need it for a customer.

Kind regards,

Danko

    This topic has been closed for replies.

    1 reply

    ST Employee
    June 18, 2018
    Posted on June 18, 2018 at 16:25

    It depends on the microcontroller. If the microcontroller also support 3-wire SPI than only MOSI line is needed.