How to distinguish two different kind of movement to wake up a microcontroller
Hi everybody,
I would like to have your opinion about waking up a microcontroller using LIS3DSH sensor. I have two different motion and only one of them should wake up the controller.
The micro is a STM32L486.
The sensor is assembled on a board and the board is fixed on a metal box, only one axis has to be monitored, the box will move along Z axis with the two possible motions:
1) Vertical position is a sort of sine wave with an amplitude of only 10cm and a period of 1sec
2) straight movement for 10 second lifting the box up to 1.5m
The two motions are quite different and only the straight movement should wake up di microcontroller, do you thing this is something doable using the LIS3DSH SM embedded into the device?
Any advice will be appreciated
Thanks
Jule