how to get LSM6DSOX simple I2C pass through working
I have a MMC5603NJ (i2c addr 0x30) connected to SDx and SCx on LSM6DSOX with INT2 pin grounded. I can see with logic analyzer I2C transactions on BOTH the Slave and Master interface, but every time I try to access a register in MMC5603 on Master bus I get a NAK, as if the LSM6DSOX is not letting the SDx pin go to float maybe? seems like it "should just work" i see all the slave I2c transactions mirrored on the master SDx and SCx pins exactly, just cannot access the other device on the master side of the LSM. I must be doing sometime (simple) wrong? Also .. how do you configure the "Modes" 1,2, on this chip? is it only by vitrue of the wiring ? thanks much