How to get rid of audio spike of MP34DT06JTR in STEVAL-BCNKT01V1. and and the frequency response does not follow the specification. + Power issue
Hi,
I am working with STEVAL-BCNKT01V1 (Bluecoin board) with the sample project FP-SNS-ALLMEMS1 and BlueMS for android (with default configuration.) I found that there are many spikes in the mic signal occurring every 20-70ms. To make sure the hardware working well, I ordered another one, but the result was the same. Does anyone have the problem similar to me and how to fix this problem?
Further more, since I have to work with low frequency under 150Hz, which the datasheet of MP34DT06JTR says it should work well to 100Hz (very small different to the frequency of 1kHz). (Actually, I need down to 50Hz.) However, I barely detected the signal under 200Hz. I tried to test with pure sine wave sound of under 500Hz. At 500Hz, it worked perfectly. At 200Hz, significant distorted waveform was detected. And I could not detect at all at 140Hz. Could anyone confirm the performance under specification of MP34DT06JTR ?
I also found that, frequently, I could not turn on the Bluecoin board (with/without battery). The power LED blinked for a half second and shut itself. Sometime, the four LEDs blinks for a time and then shut itself down again. Do you have any suggestion regarding this problem?
PS. It seems IC chips from ST are shortage, My project schedule is now ruined due to the lack of ICs (ARM) in the market. Do you know when I can make an order again? The suppliers say I have to wait for a year!!
Best regards,
Taweechai