How to make the LSM6DSOX run ultra-low-power in production environment?
Hello all,
I've recently been trying to make the LSM6DSOX run ultra-low-power. However, I can't get it to work. I tried it with the 109V3 dev board in Unico, where I can get it to run at ~15uA. However, when I turn that configuration into a .h (header) file and load it into my project, it does not work. The LSM runs at 170+ uA and doesn't even give interrupts.
Do I have to change the settings of the LSM in my code like:
/* Turn off Sensors */
lsm6dsox_xl_data_rate_set(&dev_ctx, LSM6DSOX_XL_ODR_OFF);
lsm6dsox_gy_data_rate_set(&dev_ctx, LSM6DSOX_GY_ODR_OFF);
/* Disable I3C interface */
lsm6dsox_i3c_disable_set(&dev_ctx, LSM6DSOX_I3C_DISABLE);
/* Enable Block Data Update */
lsm6dsox_block_data_update_set(&dev_ctx, PROPERTY_ENABLE);
/* Set full scale */
lsm6dsox_xl_full_scale_set(&dev_ctx, LSM6DSOX_4g);
lsm6dsox_gy_full_scale_set(&dev_ctx, LSM6DSOX_2000dps);
/* Route signals on interrupt pin 1 */
lsm6dsox_pin_int1_route_get(&dev_ctx, &pin_int1_route);
pin_int1_route.mlc1 = PROPERTY_ENABLE;
lsm6dsox_pin_int1_route_set(&dev_ctx, pin_int1_route);
/* Configure interrupt pin mode notification */
lsm6dsox_int_notification_set(&dev_ctx, LSM6DSOX_BASE_PULSED_EMB_LATCHED);
/* Set Output Data Rate.
* Selected data rate have to be equal or greater with respect
* with MLC data rate.
*/
lsm6dsox_xl_data_rate_set(&dev_ctx, LSM6DSOX_XL_ODR_26Hz);
lsm6dsox_gy_data_rate_set(&dev_ctx, LSM6DSOX_GY_ODR_OFF);Or are these settings included in the .h file I produce from Unico?
Thanks!