How to set ATime, MTime and FrTime parameters to calculate position with low error
Hi,
I modified the example program "Data Log Fusion" to calculate the position by integrating twice the linear acceleration. However, there is an error on linear acceleration that is very consistent both when the board is moving and the board is stationary. I read that ATime, MTime and FrTime are the parameters which most influence the behaviour of the MotionFX algorithm. Is there a method to set those parameters properly?
I use Nucleo-L476RG with X-NUCLEO-IKS01A2.
Waiting for a reply.
Thanks,
Marco Perciavalle