How to set up and read SFLP Game Vector on ISM330BX
Hello,
I am developing a custom application that uses your ISM330BX IMU. I am communicating with the IMU using I2C. I checked that I can commuicate correctly with it by requesting the ID in the WHO_AM_I register and everytihng seems to work fine.
The end goal is to get the LPSF block to work and output data to the fifo where it's going to be read by the main MCU. So far I tried following the info in the datasheet and the application note AN6109, but with little success. Every time I try to read the TAG of the data in the FIFO, the IMU always returns 0x02.
Please find below (and attached) the two functions I use to set up the IMU and read from the FIFO. I am sure I might have missed something in the configuration, but I can't seem to figure out what.
Thanks for the help.
Kind regards,
Marco
// accel/gyro control
#define CTRL1_XL 0x10 // XL ODR & mode :contentReference[oaicite:1]{index=1}
#define CTRL2_G 0x11 // G ODR & mode :contentReference[oaicite:2]{index=2}
#define CTRL3_C 0x12 // BDU, auto-inc :contentReference[oaicite:3]{index=3}
#define CTRL6 0x15 // G full-scale (FS_G) :contentReference[oaicite:4]{index=4}
#define CTRL8_XL 0x17 // XL full-scale (FS_XL) :contentReference[oaicite:5]{index=5}
// embedded functions (sensor fusion)
#define FUNC_CFG_ACCESS 0x01 // enable access to EMB_* :contentReference[oaicite:6]{index=6}
#define EMB_FUNC_EN_A 0x04 // SFLP_GAME_EN bit :contentReference[oaicite:7]{index=7}
#define EMB_FUNC_INIT_A 0x66 // SFLP_GAME_INIT bit :contentReference[oaicite:8]{index=8}
#define SFLP_ODR 0x5E // SFLP low-power ODR :contentReference[oaicite:9]{index=9}
#define EMB_FUNC_FIFO_EN_A 0x44 // batch SFLP data in FIFO :contentReference[oaicite:10]{index=10}
#define PAGE_RW 0x17
#define PAGE_SEL 0x02
#define PAGE_ADDRESS 0x08
#define PAGE_VALUE 0x09
// FIFO control
#define FIFO_CTRL1 0x07
#define FIFO_CTRL2 0x08
#define FIFO_CTRL3 0x09
#define FIFO_CTRL4 0x0A
#define FIFO_STATUS1 0x1B
#define FIFO_STATUS2 0x1C
// FIFO-output registers
#define FIFO_DATA_OUT_TAG 0x78 // tag byte :contentReference[oaicite:11]{index=11}
#define FIFO_DATA_OUT_BYTE_0 0x79
#define FIFO_DATA_OUT_BYTE_1 0x7A
#define FIFO_DATA_OUT_BYTE_2 0x7B
#define FIFO_DATA_OUT_BYTE_3 0x7C
#define FIFO_DATA_OUT_BYTE_4 0x7D
#define FIFO_DATA_OUT_BYTE_5 0x7E
// tag for “game” rotation vector in FIFO
#define TAG_SFLP_GAME_ROT 0x13 // 0x13 = quaternion vector tag :contentReference[oaicite:12]{index=12}
// scale: raw → Q component (unit-less). ST uses Q14 → divide by 2^14
#define SFLP_QUAT_LSB (1.0f/16384.0f)
void imu_init(void){
uint8_t t;
MXC_GPIO_OutClr(gpio_ch_sel_out.port, gpio_ch_sel_out.mask);
MXC_Delay(MXC_DELAY_USEC(20));
// Fully reeset device through SW_POR
writeRegister(I2C_MCU_ADDR, FUNC_CFG_ACCESS, (uint8_t)(0x01<<2), 1); //parameters are IMU_ADDR, REG2WRITE, DATA2WRITE, DATA LEN IN BYTES
MXC_Delay(MXC_DELAY_MSEC(50));
// From Application Note AN6109 page 57
writeRegister(I2C_MCU_ADDR, FUNC_CFG_ACCESS, 0x80, 1);
writeRegister(I2C_MCU_ADDR, PAGE_RW, 0x40, 1);
writeRegister(I2C_MCU_ADDR, PAGE_SEL, 0x01, 1);
writeRegister(I2C_MCU_ADDR, PAGE_ADDRESS, 0xD2, 1);
writeRegister(I2C_MCU_ADDR, PAGE_VALUE, 0x50, 1);
writeRegister(I2C_MCU_ADDR, PAGE_RW, 0x00, 1);
writeRegister(I2C_MCU_ADDR, FUNC_CFG_ACCESS, 0x00, 1);
//CTRL3_C: block-data-update, auto-increment
t = (1<<6) /* BDU=1 */ | (1<<2) /* IF_INC=1 */;
writeRegister(I2C_MCU_ADDR, CTRL3_C, t, 1);
writeRegister(I2C_MCU_ADDR, FIFO_CTRL3, 0x00, 1); //Prevent Accel and Gyro data from being stored to FIFO
writeRegister(I2C_MCU_ADDR, FIFO_CTRL2, 0x00, 1);
writeRegister(I2C_MCU_ADDR, FIFO_CTRL1, 0x01, 1); //Set 6 samples as max FIFO depth (2 samples for each quaternion are needed)
writeRegister(I2C_MCU_ADDR, FIFO_CTRL4, 0x02, 1); //Set FIFO with WTM
// accelerometer:
writeRegister(I2C_MCU_ADDR, CTRL8_XL, 0x00, 1); //FS_XL=00→±2g
writeRegister(I2C_MCU_ADDR, CTRL1_XL, 0b0111, 1); // ODR_XL=0111→240Hz, high-perf;
// gyroscope:
writeRegister(I2C_MCU_ADDR, CTRL6, 0x00, 1); // set FS_G=0000→±125dps
writeRegister(I2C_MCU_ADDR, CTRL2_G, 0b0111, 1); // ODR_G =0111→240Hz, high-perf;
// access embedded-function page
writeRegister(I2C_MCU_ADDR, FUNC_CFG_ACCESS, 0x80, 1);
// enable sensor-fusion LP block
writeRegister(I2C_MCU_ADDR, EMB_FUNC_EN_A, 0b0100, 1); // SFLP_GAME_EN = bit2
// set SFLP ODR to 120Hz: bit6=1, bits5-3=011, bit2=0, bit1-0=11
t = (1<<6) | (0b011<<3) | 0x03;
writeRegister(I2C_MCU_ADDR, SFLP_ODR, t, 1);
// batch quaternions into FIFO
writeRegister(I2C_MCU_ADDR, EMB_FUNC_FIFO_EN_A, 0b0010, 1); // SFLP_GAME_FIFO_EN = bit1
// reinit SFLP state machine
writeRegister(I2C_MCU_ADDR, EMB_FUNC_INIT_A, 0b0010, 1); // SFLP_GAME_INIT = bit1
// leave embedded-function page
writeRegister(I2C_MCU_ADDR, FUNC_CFG_ACCESS, 0x00, 1);
return;
}
int imu_read_quaternions(void){
MXC_GPIO_OutClr(gpio_ch_sel_out.port, gpio_ch_sel_out.mask);
MXC_Delay(MXC_DELAY_USEC(20));
if(readRegister(I2C_MCU_ADDR, FIFO_DATA_OUT_TAG, 1) != 0){ //parameters are IMU_ADDR, REG2READ, N BYTES TO READ
return 1;
}
//The rxdata buffer contains the data received from the I2C slave
if ((rxdata[0] & 0x1F) != TAG_SFLP_GAME_ROT) {
readRegister(I2C_MCU_ADDR, FIFO_DATA_OUT_BYTE_0, 6);
return 2; // not a quaternion sample
}
if (readRegister(I2C_MCU_ADDR, FIFO_DATA_OUT_BYTE_0, 6) != 0) {
return 3;
}
Stxdata[0] = rxdata[1];
Stxdata[1] = rxdata[0];
Stxdata[2] = rxdata[3];
Stxdata[3] = rxdata[2];
Stxdata[4] = rxdata[5];
Stxdata[5] = rxdata[4];
Stxdata[6] = CRC8(Stxdata, 6);
return 0;
}