Skip to main content
Explorer
May 19, 2025
Solved

How to use AH_QVAR on STEVAL MKI250KA

  • May 19, 2025
  • 1 reply
  • 394 views

Hi, I have STEVAL MKI109D, on it I mounted STEVAL MKI250KA. I would say if I could use QVAR Swipe Electrode mounted on STEVAL MKI250KA for reading Qvar signal. It is possible?

    This topic has been closed for replies.
    Best answer by Federica Bossi

    Hi @Luisa_97 ,

    Series capacitors CS1 and CS2 are used to remove DC voltage. By replacing these capacitors with a short, it can be used for UI applications (it is recommended to set the gain to 16x to ensure saturations).

    1 reply

    ST Employee
    May 20, 2025

    Hi @Luisa_97 ,

    In order to use QVAR Swipe electrode on STEVAL MKI250KA there are some modification that have to be implemented, otherwise for QVAR functionalities you can use MKI235KA.

    Hope this could help.

    Luisa_97Author
    Explorer
    May 20, 2025

    Hi @casadeib ,

    Could you specify what modifications are required? I am usinf MKI235KA, but I would like to compare the signals recorded from both devices in MEMS-Studio to observe any differences. 

    Thanks.

    Technical Moderator
    May 26, 2025

    Hi @Luisa_97 ,

    Series capacitors CS1 and CS2 are used to remove DC voltage. By replacing these capacitors with a short, it can be used for UI applications (it is recommended to set the gain to 16x to ensure saturations).