How to use the FP-SNS-MOTENVWB1 with STM32CubeIDE?
The archive downloaded here contains projects for various IDEs, including the STM32CubeIDE.
The project compiles and runs fine with the P-Nucleo-WB55 and the X-NUCLEO-IKS01A3 sensor shield.
When trying to add a timer in the Cube configuration, it throws off the files in the project, creates duplicates and the project does not compile anymore.
- Am I using the STM32CubeIDE correctly? Should I be using the CubeMX instead?
- Why does the Project Explorer folder structure is totally different than the file system structure?
Using STM32CubeIDE 1.1.0 on a Windows 10 machine.
Thanks