How to use the high pass filter in LIS3DHTR?
Hi, I'm using the LIS3DHTR and I read the applications note and the datasheet, but after that I'm still no understanding how to use the high pass filter, so I have some questions.
1-The purpose of the high pass filter is to filter de DC component?
2-I read that 2 modes exits, but in the application note AN3308 explains that there are 4 modes. Could you explain exactly what each mode do and how to use them? I do not understand if I need to reed the reference register each ODR or only at the beggining and the differences between each mode.
¡Thanks !