Skip to main content
Visitor II
August 29, 2020
Question

How to use VL53L3 histogram feature?

  • August 29, 2020
  • 6 replies
  • 1674 views

I understand the VL53L3 can detect multiple objects, and I think it puts ToF information into different buckets. Where can I find more information about this? app notes, register set, driver software, evaluation code? So far I can only see the data sheet DS13204 which does not have this information.

    This topic has been closed for replies.

    6 replies

    ST Employee
    August 30, 2020

    ON ST.com search for VL53L3, and 'get software'. We supply the software so you don't have to write very much code.

    You will get to:

    STSW-IMG015

    VL53L3CX API (Application Programming Interface)

    And the users manual is in the with the code delivery.

    To answer your specific question, there is a function called something like 'GetExtraInformation' or something like that.

    ST Employee
    September 11, 2020

    Hi @charles23​ ,

    did you get the useful information you needed?

    -Eleon

    charles23Author
    Visitor II
    September 23, 2020

    Thanks for the pointer. Indeed, in the sample application the call to VL53LX_GetMultiRangingData(Dev, pMultiRangingData) returns an array of RangeData objects (up to 4), each with range and status. That is probably adequate.

    I see there is a call VL53LX_GetAdditionalData() which returns an object that has a member of type VL53LX_histogram_bin_data_t, which in turn has a member of type int32_t bin_data[VL53LX_HISTOGRAM_BUFFER_SIZE] (where VL53LX_HISTOGRAM_BUFFER_SIZE = 24). So I guess there is a lot more going on under the hood.

    That said, insight into what is going on would be interesting and possibly useful...

    ST Employee
    September 23, 2020

    A histogram adds up all the photons received within a given clock.

    So if you look at the histogram data, you can tell how long it took the light to go out and come back in.

    A lot of work is required analyze the histogram, as the laser does not turn on and off instantaneously.

    But if you feel like doing a lot of work that we have already done for you, you can have a go at the histogram data yourself.

    It's somewhat confusing as buried in the histogram data is the ambient light signature, but every other histogram array is fairly straight forward.

    • john

    Visitor II
    March 19, 2021

    John, are you saying that continuous readings of histogram data alternate between ambient and target histograms? Is there any way to distinguish between them?

    EDIT: Seems like `AdditionalData.VL53LX_p_006.number_of_ambient_bins` is a good marker of whether its an ambient measurement.

    Visitor II
    March 19, 2021

    DELETED

    ST Employee
    March 23, 2021

    Everything you need is on ST.com

    Go to st.com/TimeofFlight and find the sensor you want.

    then click on "tools and software:".

    For the L3 we have a linux Kernel driver (please don't use this if you're not a linux person).

    and we have the bare driver. Use this for running in linux user space.

    there is example code that runs on the ST Nucleo boards and lots and lots of documentation.

    • john