How to Validate the acceleration data?
We are using LSM6DSOXTR Sensor for getting the acceleration
Accelerator data coming from ST Sensors showing very high value of acceleration,
when compared to other Product such as YYY brand.
We mounted ST Sensor on an Industrial equipment, we get Acceleration data in mm/sec2 as below.
(We converted from mg to mm/sec2 by ((value in mg/1000)*9806.65) )
Y(in mm/sec2) X(in mm/sec2) Z(in mm/sec2)
8904.4382 4462.02575 5913.40995
9649.7436 5040.6181 3196.9679
10042.0096 2098.6231 696.27215
10865.7682 -961.0517 4177.6329
10669.6352 -6040.8964 3206.77455
10238.1426 -3991.30655 4001.1132
9306.51085 -1078.7315 1490.6108
9590.9037 2000.5566 98.0665
8227.77935 176.5197 -1990.74995
8727.9185 -2441.85585 3628.4605When we mount Sensor from other brand YYY , and measured vibration for same condition, we get below values.
x(in mm/sec2) y(in mm/sec2) z(in mm/sec2)
9.439 7.57 1.122
8.785 6.168 5.327
6.823 2.056 5.047
8.411 1.963 3.084
9.907 6.262 6.262
7.29 3.178 9.253
5.327 2.71 11.776
6.823 1.963 20.374
5.421 1.589 24.113
0.467 0.935 22.43There is huge difference between these values coming from 2 sensors for exactly same conditions.
We then calculated VRMS from acceleration data from ST Sensor and YYY sensor. With ST sensor it is coming abnormally high data.
Effectively we understand acceleration data coming from ST sensor is high value than it should be, but we are not sure, reason for this.
When we just keep ST sensor on stationary surface, we get acceleration data in mm/sec2 as below. (converted from mg)
X in mm/s2 Y in mm/s2 Z in mm/s2
9.80665 166.71305 -9747.8101
127.48645 166.71305 -9688.9702
176.5197 98.0665 -9620.32365
147.09975 58.8399 -9728.1968
78.4532 78.4532 -9581.09705
166.71305 88.25985 -10581.37535
-29.41995 313.8128 -9796.84335
68.64655 156.9064 -9433.9973
98.0665 156.9064 -9767.4234This looks to be very large. Can you please throw some light??
Regards,
Shivam