Skip to main content
Visitor II
January 27, 2021
Solved

How to wire STEVAL-MKI197V1 to a muRata nRF development board: WSM-BL241-ADA-008DK.

  • January 27, 2021
  • 2 replies
  • 1569 views

The STEVAL-MKI197V1 has standard breadboard pins on it. The muRata dk (WSM-BL241-ADA-008DK) has available connection points in position JP4 - looks like the right place to attach. Is there a ribbon cable or adapter to connect these two boards together?? thank you! (see photos)

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi @BGrap.1​ ,

    the STEVAL-MKI197V1 -and in general the DIL24 connector of ST sensors' STEVALs- has been designed to be compatible with the STEVAL-MKI109V3 motherboard (and the X-Nucleo expansions for the Sensors).

    I don't think that the schematics are immediately compatible, but if you could remap the functions of the muRata nRF according to STEVAL-MKI197V1 schematic, you could make the two boards compatible.

    -Eleon

    2 replies

    ST Employee
    January 27, 2021

    Hi @BGrap.1​ ,

    the STEVAL-MKI197V1 -and in general the DIL24 connector of ST sensors' STEVALs- has been designed to be compatible with the STEVAL-MKI109V3 motherboard (and the X-Nucleo expansions for the Sensors).

    I don't think that the schematics are immediately compatible, but if you could remap the functions of the muRata nRF according to STEVAL-MKI197V1 schematic, you could make the two boards compatible.

    -Eleon

    BGrap.1Author
    Visitor II
    January 29, 2021

    Thanks for the fast reply. We did see the DIL24 connector on the motherboard (STEVAL-MKI109v3) and considered that but thought we would reach out to anyone who might have manually wired them together.

    thanks!

    Brian